2019-02-11 4:36 AM
STM32F0x1 do not support different sampling time for different channel, what should be the configuration if i want to sample other external ADC signal with high sampling frequency with Sampling time 1.5 ADC clock cycle.
2019-02-11 4:43 AM
Use a device with two ADC peripherals, or skip the temperature channel entirely.
The chip die temperature is not really of much use in most cases.
Or add a cheap external sensing element. With proper calibration, a simple PN junction (diode) in formward direction will do.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.