2022-10-05 5:48 PM
Currently any one of the CAN channel is Working at a time.
Out customer requirement is, they need both CAN channel's need to work at the same time.
Please can you explain me and If you have sample code, please attach here.
2022-10-05 6:32 PM
The device only has one CAN controller, you're simply switching the pin mapping to use different pairs
You'll need a part with 2x CAN controllers if you need two
2022-10-06 10:19 AM
Ok Can you send me the part number of 2x CAN controllers with same pin compatibility. So we directly replace the part and check.
2022-10-06 10:24 AM
There's no 2xCAN STM32 model in QFP-48.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.