2023-01-19 1:39 PM
For example: 1000: is Combined PWM Mode, 1111: is Asymmetric PWM Mode 2.
How do you fit 4 bits into 3 bit spaces?
Bit 7 is used for OC1CE, and Bit 3 is used for OC1PE so there is no space on either end for the extra bit.
Solved! Go to Solution.
2023-01-20 5:59 AM
Ha! You are right. There is nothing in the text of the description of of OCM1 to look for the 4th bit elsewhere.
Thanks,
Kip
2023-01-19 1:55 PM
I just checked RM0390 Rev 6 page 568/1347 and it has only 8 options for the 3 bits. Which makes sense.
2023-01-19 2:28 PM
2023-01-20 5:59 AM
Ha! You are right. There is nothing in the text of the description of of OCM1 to look for the 4th bit elsewhere.
Thanks,
Kip
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.