2021-08-30 4:58 AM
I am trying to run the demo code provided by for nucleo 411RE to BNO080. I am running it in the STM32CubeIDE , but the code was written for IAR IDE.....
I tried running that code after adding necessary file but when I try
ret = HAL_I2C_IsDeviceReady(&hi2c1,0x4A<<1, 1, 100);
the ret value is always 1. i.e the connection is not established .
SW2-0
SW4-0
SW6-0
I have set all the values to 0 for i2c communication.
Suggest me some idea?
2021-08-30 10:34 AM
> Suggest me some idea?
Verify slave address is correct (default is 0x4B). Verify pins are being initialized in the correct AF mode. Verify pins on the board are available and exposed at the locations you think they are in the schematic or user manual. Verify external pullups on SDA/SCL are present. Verify target chip has power. Get a logic analyzer on the pins and see what's happening.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.