STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Outsourcing to United States

I am working on a startup, outsourcing AI and IoT focused on embedded systems, from South America (Argentina) to the United States, we are looking for a beachhead market, I have a few questions, any advice will be very appreciated:- What ecosystems, ...

dhs by Senior
  • 1848 Views
  • 3 replies
  • 0 kudos

MAX11212 interfacing with stm32l053

Hey Guys , I am trying to interface MAX11212 adc with stm32l053 controller. But i am not getting any data on my RX buffer. Details about max1121218 bit adctwo pin spi moudule with clock and dout pin24 clock cycles required to send data o...

NBhar.1 by Associate II
  • 1405 Views
  • 2 replies
  • 0 kudos

I2C connection is not established to BNO080 dev board

I am trying to run the demo code provided by for nucleo 411RE to BNO080. I am running it in the STM32CubeIDE , but the code was written for IAR IDE.....I tried running that code after adding necessary file but when I tryret = HAL_I2C_IsDeviceReady(&h...

AR.7 by Associate II
  • 1394 Views
  • 1 replies
  • 0 kudos

Fast I2C with DMA transfer issue

Hello, I have successfully implemented the standard I2C protocol with OLED. To speed up the display operations, I increased the speed of the I2C and it works fine up to 290 kHz.The protocol relies on DMA transfer and the CPU is in SLEEP until the DMA...

LaoMa by Associate III
  • 8530 Views
  • 19 replies
  • 0 kudos

How use external trigger SDADC correctly of STM32F3 ?

Hi everyone ! I want configure external trigger of sdadc in stm32373c-eval. Trigger external is TIM13 configured at 1700Hz (purple signal), when HAL_SDADC_InjectedConvCpltCallback execute i did that toggle LED and the toggle is doing 16's in one peri...

0693W00000Dlc4CQAR.jpg
BarcaM by Associate II
  • 1340 Views
  • 0 replies
  • 0 kudos

How to use the crypto library on M4-core of the STM32H757?

Hi,I tried to use the crypto library "STM32CryptographicV3.1.1_STM32H7_IARv8_otnsc.a" on the M4-core of the STM32H757 but I got some troubles as explain below. First of all, I'm using IAR 9.10 and I haven't problem when using the library on M7-core. ...

Byann.1 by Associate II
  • 4783 Views
  • 7 replies
  • 0 kudos

motionstudio2 window application connection error

I tried connecting the bno080 with nucleo 411RE using motionstudio2 window application to read the data from bno080.....I saved the flash memory for running this application and flashed the stm with another program...I flashed the application running...

AR.7 by Associate II
  • 960 Views
  • 0 replies
  • 0 kudos

how to measure force of motor

i need to measure force of a motor but i don't know i how to measure .please any one help me i'm using 24v dc motor with encoderand stm32f446re controller

LOGU by Associate II
  • 1470 Views
  • 2 replies
  • 0 kudos

c++ project in keil IDE

Hi,I'm trying to write some c++ code in keil for stm32. I have successfully written C code that compiled well but I can't create a c++ project.anyone has experience with it?

EPora.1 by Associate II
  • 847 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.