2021-09-07 10:57 PM
Dear Sir,
we are using STM32G series controller in our project but the problem is that we are also using eMMC card with 4GB which work on SDIO connectivity.
could you plese share me which STM32g series will be suitable for it.
Thank you
Solved! Go to Solution.
2021-09-08 6:47 AM
Neither the STM32G0 nor the STM32G4 families support SDMMC operation. However, you could use the card in SPI mode at reduced bandwidth. Both families can do SPI.
2021-09-08 6:47 AM
Neither the STM32G0 nor the STM32G4 families support SDMMC operation. However, you could use the card in SPI mode at reduced bandwidth. Both families can do SPI.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.