2026-01-20 10:45 PM
Hi,
we are planning to use STM32H742xI/G controller in our design, we have reviewed the datasheet and need a clarification on the IO logic for QSPI.
Does this controller supports 1.2v IO logic for the QSPI.
Solved! Go to Solution.
2026-01-21 12:16 AM
Hello @saminathan and welcome to the community;
Unfortunately, 1V2 IO logic for QUADSPI interface isn't supported. Please look at this post.
This request is already shared with expert.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-21 12:16 AM
Hello @saminathan and welcome to the community;
Unfortunately, 1V2 IO logic for QUADSPI interface isn't supported. Please look at this post.
This request is already shared with expert.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-01-21 2:50 AM
Hi @KDJEM.1,
Ok as suggestion, we are going to plan to use bi-directional level translator SN74AXC4T245PWR.
Does it work if we use level translator?
Thanks,
Saminathan
2026-01-21 3:01 AM
Hello @saminathan ;
To verify whether it is functional or not, you need to check that the signals required for SN74AXC4T245PWR must be compatible with the QUADSPI signals.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.