2026-01-21 1:10 AM - last edited on 2026-01-21 1:43 AM by mƎALLEm
2026-01-21 1:18 AM
> Is VREFINT and VREFBUF output same?
No.
> In documents I have seen VREFBUF can be set as 2.048, 2.5, 2.9, is that same VREFINT?
No.
JW
2026-01-21 1:22 AM
Hi @waclawek.jan,
Could you please mention the purpose of that VREFBUF and VREFINT?
2026-01-21 1:41 AM - edited 2026-01-21 1:43 AM
VREFINT is a fixed nominally 1.2V internal reference, which you can measure using the ADC, and thus indirectly establish voltage of the ADC's reference (ADC reference is always the VREF+ pin). Read the Monitoring the internal voltage reference subchapter of ADC chapter in RM0440.
VREFBUF is a voltage source with selectable voltage, which can internally be connected to VREF+ pin (but if you want to do that, you must not connect an external source to VREF+, but you must connect a prescribed capacitor to VREF+ - see datasheet). Read the Voltage reference buffer (VREFBUF) chapter in RM0440.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.