2022-02-09 10:32 AM
2022-02-09 3:03 PM
If you can connect to the chip, it's probably fine, especially as PC13 works. Verify LED polarity. What pin are you trying to use? Verify the hardware connection is there.
Always a possibility that a pin is damaged, but they don't damage themselves. Had to be an event that caused it.
2022-02-10 12:25 AM
What if the LED yure trying to connect is broken or with the wrong polarity?
2022-02-10 2:35 AM
Well, I have already made sure of that. I connected an external 3.3v and it works well
2022-02-10 2:37 AM
The LED is working well and i already made sure of that. But with alot of testing i figured out that the problem is in the GND pins of the MCU somehow.
2022-02-10 2:40 AM
I used the GND of the st link programmer and tried all of GPIO pins and it worked.
For some reason the GND of the MCU is not working.
2022-02-10 8:15 AM
if your internal PC13 (green if youre using a bluepill) is working and your external LED is not , there is a hardware/wiring problem.
Could you show us your setup?(pìctures)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.