STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 9-bit UART data not as expected

HiWe are using the STM32L4S7AI. We have USART2 configured as 9-bit data.We are using the HAL and have been using 8-bit HAL on many STM32 for a while... this is our first 9-bit data use.We set UART_InitTypeDef.WordLength to UART_WORDLENGTH_9B.On the w...

0693W00000JPNK5QAP.png 0693W00000JPNKUQA5.png

I2C driver code generation from scratch.

Hi team, I am trying to generate I2C driver code using STM32CubeIDE, to understand perpheral functions. I was successful in generating the code but i cant find the functions which I am looking for like I2C_Init(), I2C_cmd, I2C_GetFlagStatus() ...Coul...

IJose.1 by Associate II
  • 12622 Views
  • 9 replies
  • 0 kudos

Is it correct that HAL_UART_RxHalfCpltCallback and HAL_UART_RxCpltCallback are invoked even when there is nothing connected to the Tx and Rx pins of my microcontroller?

Hi community!I would like to understand if it is normal that when I use DMA method to receive data the callback related to this method are invoked even when there is nothing connected to the Tx and Rx pins of my microcontroller.I'm using a NUCLEO-F30...

VNava.1 by Associate III
  • 3491 Views
  • 9 replies
  • 0 kudos

using internal Vrefbuf : HAL Code generation issue

I try to VREFPIN in internal mode (so VREFPIN is an output).Based on IDE STM32CUBEIDE 1.3.0 and using a STM32G071 MCU.The generated code is : void HAL_MspInit(void){ __HAL_RCC_SYSCFG_CLK_ENABLE(); __HAL_RCC_PWR_CLK_ENABLE(); /* System interrupt init...

THAUS.1 by Associate
  • 2475 Views
  • 1 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.