2020-11-22 8:21 AM
Hi.
I am working with a mcu stm32f030k6
.
My problem is that I can not protect my memory reading.
I used a few code samples but got no results.
Is there a solution?
Using with writing code of the the main mcu or
This can be done through the programmer J-link
Thank you very much for your help.
An example of my code that That did not work and does not run mcu
main{
ReadProtectionConfig (1)
}
uint8_t ReadProtectionConfig(uint8_t ProtectionLevel)
{
uint8_t status = 0;
FLASH_OBProgramInitTypeDef OB_Init;
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
OB_Init.OptionType = OPTIONBYTE_RDP;
if (ProtectionLevel == 0) {
OB_Init.RDPLevel = OB_RDP_LEVEL_0;
} else if (ProtectionLevel == 1) {
OB_Init.RDPLevel = OB_RDP_LEVEL_1;
} else if (ProtectionLevel == 2) {
OB_Init.RDPLevel = OB_RDP_LEVEL_2;
} else {
status = 1;
return status;
}
HAL_FLASHEx_OBProgram(&OB_Init);
HAL_FLASH_OB_Launch();
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
return status;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.