2021-01-05 6:38 AM
Using STM32F767ZI,
Note:- I have comment some of the statements
2021-01-05 10:16 AM
This doesn't look like code for an STM32. It looks like it's for a TI chip, if I had to guess.
DDRD |= (1 << D_RESET) | (1 << D_IN); //PD3, PD5 output (output to D-ff /RESET and D-in)
D_FF_PORT |= (1 << D_CLK) | (1 << ICP); //PD4, PD6 pull up (inputs for resp. T0 en ICP)
DDRB |= (1 << SPI_CLK) | (1 << SPI_DO) | (1 << SPI_CE); //PB0,1,2 output (to MAX7219)
DDRB |= (1 << LED); //PB3 output
SPI_PORT |= (1 << SPI_CE); //set CE high
TCCR0A = 0; //normal mode
TCCR0B |= (1 << CS02) | (1 << CS01) | (1 << CS00); //clock input extern, RISING edge
TIMSK |= (1 << TOIE0); //interrupt bij overflow
TCCR1A = 0; //normal mode
TCCR1B |= (1 << CS10); //prescaler = 1 (10MHz)
TCCR1B |= (1 << ICES1); //input capture on RISING edge
TCCR1C = 0;
TIMSK |= (1 << TOIE1) | (1 << ICIE1); //enable interrupt on overflow & input capture
...
ISR (TIMER0_OVF_vect) //TIMER0 overflows after 256 counts
{
input_counter_high++;
}
2021-01-05 10:20 AM
Not making a particularly strong presentation.
Unrelated main.c, AVR project?
stm32f7xx_hal_msp.c not showing how the ARR is read from the TIM, looks to be using an unrelated DMA resource.
Which source trigger? Which counter is read? Where is it written?
ZIP up a project that's actually compilable.
With this type on endeavour it is important to connect all the dots properly, making random selections is bound to fail.
2021-01-06 11:07 PM
2021-01-07 3:48 AM
What's the hardware? What's the trigger source pin? Does that pin work, ie. if you set it as plain GPIO input and observe it in debugger, do you see it changing in IDR as the input level changes? In the "full code", is the relevant CC flag in TIMx_SR set after the trigger occurs?
Where is the memory buffer allocated? Is that memory accessible by DMA? Is that a cached memory? If so, are you aware of cache coherency problems?
If answers to these questions won't help, read out and check/post the TIM, DMA and relevant GPIO registers content, after the attempt to trigger.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.