2019-05-17 12:18 AM
I have generated the code (LED PB7 GPIO_OUT) by using STM32Cube Mx for MDK ARM5. While loading the code , I am getting following error.
Contents mismatch at: 08001000H (Flash=00H Required=31H) !
I have resolve this issue by erasing the flash using ST-LINK UTILITY after that code is loading first time but it's not executing (PB7 LED not blinking) then I reconnect the USB and it seems LED PB7 blinking.
If again I am trying to dump the same code , I am getting same above error..
Can you please provide the solution to resolve this issue.
Solved! Go to Solution.
2019-05-17 3:42 AM
Go to the project options in Keil.
Select the Debbuger Settings
In the Flash tab look at the flash algorithm and then switch it for the alternate banking mode. ie if single bank mode, select dual, or reverse.
2019-05-17 3:42 AM
Go to the project options in Keil.
Select the Debbuger Settings
In the Flash tab look at the flash algorithm and then switch it for the alternate banking mode. ie if single bank mode, select dual, or reverse.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.