2026-02-05 10:07 AM
New user, fresh download of STM32CubeIDE 2.0.0.
Created the demo "hello world" c++ project. Then attempted to compile it. It fails with the message:
Error: Program "make" not found in PATH
PATH=[C:/ST/STM32CubeIDE_2.0.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.jre.win64_3.4.100.202508201254/jre/bin/server;C:/ST/STM32CubeIDE_2.0.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.jre.win64_3.4.100.202508201254/jre/bin;C:\windows\system32;C:\windows;C:\windows\System32\Wbem;C:\windows\System32\WindowsPowerShell\v1.0\;C:\windows\System32\OpenSSH\;C:\ST\STM32CubeIDE_2.0.0\STM32CubeIDE]
I have examined the contents of C:\ST\STM32CubeIDE_2.0.0\STM32CubeIDE and i dont see "make.exe" anywhere in the directory tree. Where is it? Why doesnt the IDE find it wherever it is?
Help
Solved! Go to Solution.
2026-02-05 11:42 AM - edited 2026-02-05 11:44 AM
Hello @mr_swift and welcome to the ST community,
I invite you to read this knowledge base article: STM32CubeIDE 2.0.0 workflow tutorial
Especially the section 2. New workflow with STM32CubeIDE
Hope that helps.
2026-02-05 10:17 AM
STM32CubeIDE is not set up to create fresh projects, despite whatever "new project" features are shown there.
Use the standalone STM32CubeMX to create a project and, after generating code, click "Open Project" to open it in STM32CubeIDE.
2026-02-05 11:42 AM - edited 2026-02-05 11:44 AM
Hello @mr_swift and welcome to the ST community,
I invite you to read this knowledge base article: STM32CubeIDE 2.0.0 workflow tutorial
Especially the section 2. New workflow with STM32CubeIDE
Hope that helps.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.