2025-10-24 4:01 AM
Hi I am looking into using STM32F446RCTx for my design, which includes 2 x USB FS 2.0 (1 x Host + 1 x Device). Hence need to provide an external HSE. I want to use an Oscillator, meaning I setup the HSE as "Bypass Clock Source" .
With this setup I planned to use the pin 6 (PH1_OSC_OUT) as a GPIO for other functionalities. But the STM32CubeMX setting does not let me do this.
I see that this pin will be (OSC_OUT) High Impedance as per RM0390 - Page 120. Am I right in say that I MUST leave this pin NC and cannot free up to use as GPIO?
Thanks.
Solved! Go to Solution.
2025-11-18 1:53 AM - edited 2025-11-28 1:06 AM
Hello,
I've got a confirmation from the team: yes for STM32F446 you can use OSC_OUT and OSC32_OUT as GPIOs when HSE or LSE are in bypass mode.
The documentation will be updated accordingly (Internal ticket number 220390).
Hope that answers your question.
2025-10-24 4:15 AM - edited 2025-10-24 4:23 AM
Hello,
I think that possibility is available only in newer products. STM32H7 can do that.
According to the STM32F446 reference manual. It says not. But I can check internally. Internal ticket number 220390 not accessible by the community members.
2025-10-24 5:41 AM
Hi Thanks for checking this out.
2025-10-30 5:04 AM
Hi, the answer to the original question what I should do with the OSC_OUT pin is fine for me to get on with the design for now. I am however is still waiting for the answer FROM ST on if there is a way of using this port as GPIO. Your associate mƎALLEm mentioned that he will find this out from ST.
Thanks
2025-10-30 6:06 AM - edited 2025-11-18 2:05 AM
Hello @BPart.1 ,
I'm still waiting a confirmation from the internal team. If I have any feedback I will get back to you.
Thank you for you patience.
2025-11-18 1:53 AM - edited 2025-11-28 1:06 AM
Hello,
I've got a confirmation from the team: yes for STM32F446 you can use OSC_OUT and OSC32_OUT as GPIOs when HSE or LSE are in bypass mode.
The documentation will be updated accordingly (Internal ticket number 220390).
Hope that answers your question.
2025-11-18 3:51 AM - edited 2025-11-18 3:51 AM
> yes for STM32F446 you can use OSC_OUT and OSC32_OUT as GPIOs when HSE or LSE are in bypass mode
This is interesting. I've just tested and, yes, the 'F446 is different from the 'F427 (and thus presumably also 'F407) in this detail.
I've noticed another interesting and undocumented detail: in both the 'F446 and the 'F427, the RCC_CR.HSEBYP bit appears to be not reset by Software Reset, only by NRST and Power Reset.
JW
2025-11-29 1:55 AM
Similar question here:
How to set Hi-Z mode in PH1 (OSC_OUT) when using HSE BYPASS mode in STM32F446RE?
2026-05-13 9:23 AM
@mƎALLEm wrote:The documentation will be updated accordingly (Internal ticket number 220390).
@BPart.1 It seems that CubeMX also needs an update to allow this:
2026-05-13 10:00 AM
Indeed
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.