STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Internal Oscillator Clock issue - STM32U375VGT6Q

We are using MPN: STM32U375VGT6Q in one of our projects, with the internal RC oscillator configured as the core clock source.During board validation, when the system clock was configured to the maximum frequency of 96 MHz, we observed a signal integr...

abk by Associate II
  • 634 Views
  • 5 replies
  • 1 kudos

Resolved! HSE Bypass mode - Possible use of OSC_OUT as GPIO

Hi I am looking into using STM32F446RCTx for my design, which includes 2 x USB FS 2.0 (1 x Host + 1 x Device). Hence need to provide an external HSE. I want to use an Oscillator, meaning I setup the HSE as "Bypass Clock Source" .With this setup I pla...

BPart.1 by Associate II
  • 1333 Views
  • 9 replies
  • 7 kudos

Resolved! FD-CAN - Protocol Error - ACK Error

Hello, We are facing an intermittent CAN-FD issue in the field and would appreciate guidance from the community. Our system has two devices on the bus (no other device on the bus) using a request–response architecture. The master sends a request ever...

TSola.1 by Associate II
  • 3246 Views
  • 15 replies
  • 4 kudos

Using external RAM with STM32U5G9-HSPI

Hi Everyone,I am working on a project with TouchGFX. I'm working with STM32U5G9ZJT6 and I have an external RAM APS12808L-OBM-BA connected via HSPI (Fclk-hspi 100 MHz) in mapped mode. The project is working, but the image animation are not working wel...

Carlos_Aperton_0-1763041028096.png Carlos_Aperton_1-1763041362659.png Carlos_Aperton_2-1763041490365.png Carlos_Aperton_3-1763041569967.png

Resolved! Minimizing STM32H743IIK6 current in sleep mode

If the STM32H743IIK6 is clocked by an external 25MHz clock generator, but we still aim for minimum current consumption until a wake-up is required, what is the lowest achievable current draw assuming everything is powered down except for the external...

ELI_HAIT by Associate II
  • 331 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.