2021-12-24 6:12 AM
Hello,
I'm having fun with hrtim configuration on STM32G4.
To prevent to broke my device, I implement a faults management.
I have also an external event that disable output (delayed idle mode), which can be reactivated by software when external event disappear.
So my problem is: I get the fault and deactivate hrtim timer output. But few nano second later my callback check if there is no more external event and reactivate the output while I still have the fault.
I found a software solution to avoid this but I would prefer an hard one.
I read on the reference manual RM0440 (V5), at page 928 (section 27.3.17) that hrtim had mechanisme to forbidden output activation while fault is present ("In case of a permanent fault request, the output remains in its fault state, even if the software attempts to re-enable them, until the fault source disappears").
But I can't find a way to configure it. I try with lock register without success. Some had informations about this ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.