2021-12-20 1:03 AM
I am new to microcontroller development and trying to implement my first custom ble service.
I looked at a few other examples that often use the _App_Context_t struct to store data before passing it to the character update method.
Example:
Custom_STM_App_Update_Char(CUSTOM_STM_LED_VALUE, (uint8_t *) &Custom_App_Context.LEDMeasurement.LED1_Value);However, after enabling notifications for some characteristics, cubemx also generates methods like
Custom_Led_value_Update_Char() and Custom_Led_value_Send_Notification() that send data via the UpdateCharData[247]; and NotifyCharData[247]; arrays defined at the top of the file.
Could someone explain the difference between those arrays and using a App_Context, the reason for their 247 byte length etc.?
void Custom_Led_value_Update_Char(void) /* Property Read */
{
Custom_STM_App_Update_Char(CUSTOM_STM_LED_VALUE, (uint8_t *)UpdateCharData);
/* USER CODE BEGIN Led_value_UC*/
/* USER CODE END Led_value_UC*/
return;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.