2026-01-15 11:09 AM
Hi,
I'm building a BLE application using custom template in STM32CubeMX. I have two services. The first one has only one characteristic with the properties "Read" and "Write without response". The second service has two characteristics, both with "Read" and "Notify" properties.
The code generated in "custom_app.c" have the function:
void Custom_<Srv2Char1>_Update_Char(void){...}
void Custom_<Srv2Char1>_Send_Notification(void){...}
void Custom_<Srv2Char2>_Update_Char(void){...}
void Custom_<Srv2Char2>_Send_Notification(void){...}However, no function is generated for the characteristic of the first service. I expected to have a function like this:
void Custom_<Srv1Char1>_Update_Char(void){...}
I performed some tests:
In both cases, no "Update_Char" function was generated.
I don’t know if this behavior is correct. If it is, how am I supposed to respond to a "Read" request?
Here’s what I’m doing:
void Custom_STM_App_Notification(Custom_STM_App_Notification_evt_t *pNotification)
{
switch (pNotification->Custom_Evt_Opcode)
{
...
...
case CUSTOM_STM_<Srv1Char1>_READ_EVT:
...
Custom_STM_App_Update_Char(CUSTOM_STM_<Srv1Char1>, (uint8_t*) UpdateCharData);
...
break;
...
...
}
return;
}
Some other info:
Thanks!
2026-01-15 11:16 PM - edited 2026-01-20 5:24 AM
Hello @DecaMeron
Your contribution is greatly appreciated.
A ticket has been escalated to dev team under the internal ticket number 225400 and it will be fixed as soon as possible.
I will keep you posted with updates.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.