2021-12-17 1:53 PM
Hi, I'm working on a project which involves STM32L476QEI. It has external dedicated OPAMP1_VINM and OPAMP2_VINM (M3 and M4 pins). If I'm not going to use the opamp functionality, do I have to connect them to the ground or leave them floating? What I learn from CubeMX is that I can use them to remap connections to free up GPIO. Are there other possibilities that I missed?
Solved! Go to Solution.
2021-12-19 11:24 PM
When not in use, I would recommend to connect them on GND, even if these are not digital inputs with Schmitt trigger. In the case of the BGA132, these are dedicated pins in order to minimize the bias current (see RM0351, section 23.3.3):
The dedicated pin is only available on BGA132 and BGA169 [...] package. This configuration provides the lowest input bias current (see datasheet).
Regards
/Peter
2021-12-19 11:24 PM
When not in use, I would recommend to connect them on GND, even if these are not digital inputs with Schmitt trigger. In the case of the BGA132, these are dedicated pins in order to minimize the bias current (see RM0351, section 23.3.3):
The dedicated pin is only available on BGA132 and BGA169 [...] package. This configuration provides the lowest input bias current (see datasheet).
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.