2013-04-15 5:51 AM
Hi,
I noticed in the STM32F429 documentation, that this microcontroller has up to 2MB Flash organized in two banks. How can I use them? Specifically - how should I compile programs over 1MB? I have to use some dedicated commands to switch between banks when I call function Foo() located in bank 0 from function Bar() located in bank 1? Can I use this Flash with GCC? #banks #flash #stm32f4292013-04-15 7:35 AM
No the memory is linear, 0x08000000 .. 0x081FFFFF, just configure your linker script properly, you'll be golden.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.