2013-04-15 12:42 AM
Hello friends
I am confused where to wire my encoders to stm32f4 ; I have 2 encoders from 2 motors , After I read the manual is it possible to wire the 2 encoders to the same timer and can configure them individually ? or I need two timers ? for example encoder 1 A to timer2 ch1 and B to timerch2 encoder 2 A to timer2 ch3 and B to ch4 (timer 2) is that ok ? Or do I need 2 seperate timers ? Do you suggest a direct wirring of the endoders or should I use latches? Thank you in advanced . Esat2013-04-15 4:38 AM
Each timer has a single counting element, that pretty much limits the possible use cases right there.
The availability of different channel configuration likely permits the use of different pins to resolve other conflicts.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.