2019-12-19 7:32 AM
hi everyone want to use interrupt in main.c i am using extern "C" for this purpose but its couldn't compile
/* USER CODE BEGIN 4 */
extern "C" void TIM2_IRQHandler(void) {
// Handle update interrupts (update interrupt flag is set)
if (TIM2->SR & TIM_SR_UIF) {
// Reset the update interrupt flag
TIM2->SR &= ~(TIM_SR_UIF);
// Toggle the LED
HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_14);
Flag_Angle = 1;
}
}
Error: L6200E: Symbol TIM2_IRQHandler multiply defined (by stm32f4xx_it.o and main.o).
also infinite while is executed just one time .
2019-12-19 7:46 AM
Don't think the issue is related to extern "C" usage.
The linker is complaining that you have two copies of the IRQ Handler's body function, both in stm32f4xx_it.c and main.c decide which one you want, and comment out the other.
Don't write TIM->SR with a RMW instruction, just WRITE the bit mask to clear the interrupt sources. See Reference Manual, read specific functionality of the register described there.
2019-12-19 8:00 AM
thanks a lot can i use IRQ Handler in main.c instead of stm32f4xx_it.c if i comment it in stm32f4xx_it.c is it a right approach and why while infinite loop execute just one time .
2019-12-19 9:43 AM
You can put it in whatever source file you choose.
>>.. why while infinite loop execute just one time .
No idea what you're talking about, lack any real context, see no code presented with a while() loop
Code lacking appropriate handlers may dump into Default_Handler(), HardFault_Handler(), or Error_Handler()
If the interrupt rate is too high (say >400 KHz) the system may saturate and continually reenter the IRQHandler, and prevent foreground execution.
2019-12-19 10:10 AM
"extern C" is for C++. It tells the compiler that the function is extern and C instead of C++ (calling convention and name mangling).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.