2023-12-14 9:59 PM
i use LCD-TFT display in microcontroller STM32H757.
i need to store framebuffer data in extern sram(S61WV102416BLL)
i use stm32H757i_evk board.
i download example code, all example code use External sdram(IS42S32800J) to store framebuffer.
i not use External sdram(IS42S32800J).
give me any example code that use extern sram(S61WV102416BLL) to store frame buffer.
otherwise you give what change required for example code use External sdram(IS42S32800J).
and we can use use extern sram(S61WV102416BLL) to store frame buffer.
please help me.
2023-12-15 2:48 AM
Hello @khodifadlalit and welcome to ST Community ,
If you want an example using S61WV102416BLL you can start from the example provided in the STM32CUBEL4
for the stm32l476-eval(STM32Cube_FW_L4_V1.18.0\Projects\STM32L476G-EVAL\Examples\FMC\FMC_SRAM) board and port it on the stm32H757i_evk board this could be found by downloading the STM32CUBEL4 or via this Github link .
BR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.