cancel
Showing results for 
Search instead for 
Did you mean: 

How to revive a dead MCU in-circuit?

Mark Williamson
Associate II
Posted on December 18, 2016 at 15:11

Hello all!  How's this for my very first question

I purchased a 3d Printer on clearance with a tag that says Does not Start up.  No warranty.  I was ok with that.  As I'm a developer and a hardware hacker I knew I was buying a project not a printer.  I have experience with Atmel, wrote my own firmware for a Cricut cutting machine, so I'm comfortable here.

The situation I believe is that the store had upgraded the firmware on this machine but used the wrong firmware.  There is much discussion about this situation on the internet from this particular brand of printers. Overall, the quality of the printer is great.  So now the problem.

The images show that the MCU is an STM32F407ZTG6.  I can see clearly that it has SWD header yay.  So I connected the STLink board from my Nucleo to it, removing the jumpers so that I can use it to program an external device, connected the 3.3v power pad on the 3D Printer's board to the 3v3 header on the Nucleo, and I can tell the board has power.  However, STLink does not see the target.  Anyone have some ideas to help revive this guy?

This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
AVI-crak
Senior
Posted on March 17, 2017 at 14:55

And shall be.

This system contains the loader - which can't be read, and the encoded firmware of level of the user - for independent filling in the processor.

Otherwise competitors will launch mass release of the copy of the similar printer - in one day.

It is possible to erase a firmware and the loader and to receive a spiritualistic board of development. For a call of spirit of the dead printer.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.