2015-06-19 8:44 AM
Hello I have a problem with the vector table relocating, I moved the vector table with the following code, but when I am activating the usart interrupts the programs hangs
#define APPLICATION_ADDRESS (uint32_t)0x08003000 __IO uint32_t VectorTable[48] __attribute__((at(0x20000000))); int main (void){ uint32_t i = 0;/* Relocate by software the vector table to the internal SRAM at 0x20000000 ***/ /* Copy the vector table from the Flash (mapped at the base of the application load address 0x08003000) to the base address of the SRAM at 0x20000000. */ for(i = 0; i < 48; i++) { VectorTable[i] = *(__IO uint32_t*)(APPLICATION_ADDRESS + (i<<2)); } /* Enable the SYSCFG peripheral clock*/RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); /* Remap SRAM at 0x00000000 */SYSCFG_MemoryRemapConfig(SYSCFG_MemoryRemap_SRAM); init_SystickClock(); rtc_ini(); init_SPI1(); init_led(); init_LCD (); Delayms(500); init_USART1(9600);}void init_USART1(uint32_t baudrate) // this funcion initializes the USART1 peripheral{ // RCC_ClocksTypeDef RCC_Clocks; GPIO_InitTypeDef GPIO_InitStructure; // this is for the GPIO pins USART_InitTypeDef USART1_InitStructure; // this is for the USART1 initilization// //************ Enable USART CLOCK ************// RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); /* GPIOA Periph clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); //************ Configure the TX and RX PIN ************// GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9|GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); //************ Configure the RTS PIN ************// GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_Init(GPIOA, &GPIO_InitStructure); //************ Configure the CTS PIN ************// GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); //************ Asigned the AF (connect USART1 pins to USART1 alternate function) ************// GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1); // TX GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1); // RX GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_1); // CTS GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_1); // RTS USART1_InitStructure.USART_BaudRate = baudrate; // the baudrate is set to the value we passed into this init function USART1_InitStructure.USART_WordLength = USART_WordLength_8b; // we want the data frame size to be 8 bits (standard) USART1_InitStructure.USART_StopBits = USART_StopBits_1; // we want 1 stop bit (standard) USART1_InitStructure.USART_Parity = USART_Parity_Even; // we don't want a parity bit (standard) USART1_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_RTS_CTS; // we don't want flow control (standard) USART1_InitStructure.USART_Mode = USART_Mode_Tx|USART_Mode_Rx; // we want to enable the transmitter and the receiver USART_Init(USART1, &USART1_InitStructure); // again all the properties are passed to the USART_Init function which takes care of all the bit setting // finally this enables the complete USART1 peripheral RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10; // Pins 9 (TX) and 10 (RX) are used GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; // the pins are configured as alternate function so the USART peripheral has access to them GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; // this defines the IO speed and has nothing to do with the baudrate! GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; // this defines the output type as push pull mode (as opposed to open drain) GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; // this activates the pullup resistors on the IO pins GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1); // GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1); USART1_InitStructure.USART_BaudRate = 9600; // the baudrate is set to the value we passed into this init function USART1_InitStructure.USART_WordLength = USART_WordLength_9b; // we want the data frame size to be 8 bits (standard) USART1_InitStructure.USART_StopBits = USART_StopBits_1; // we want 1 stop bit (standard) USART1_InitStructure.USART_Parity = USART_Parity_Even; // we don't want a parity bit (standard) USART1_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; // we don't want flow control (standard) USART1_InitStructure.USART_Mode = USART_Mode_Tx | USART_Mode_Rx; // we want to enable the transmitter and the receiver USART_Init(USART1, &USART1_InitStructure); USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); // enable the USART1 receive interrupt USART_ITConfig(USART1, USART_IT_TXE, ENABLE); // enable the USART1 interrupt //USART_ITConfig(USART1, USART_IT_RTO, ENABLE); // enable the USART1 timeout interrupt// USART_SetReceiverTimeOut(USART1, 200); GPIO_ResetBits(GPIOA,GPIO_Pin_12);// RTS Usart1 USART_Cmd(USART1, ENABLE);}2015-06-19 9:07 AM
Probably shouldn't permit it to leave main()
Review the USART IRQ, if you don't service that TXE interrupt you've enabled it will be stuck there for ever.Can you use a debugger? Where does the processor get stuck up? Does the vector table at 0x00000000 and 0x20000000 look valid?How do you get to the code at 0x08003000, have you confirmed that works?Is the code actually built to reside at 0x08003000, and have you confirmed that by reviewing the .MAP file, to confirm the placement of the image and the vector table definition you've provided?2015-06-19 1:22 PM
2015-06-19 1:42 PM
You need to prove that the vector table is correctly instantiated.
2015-06-19 7:13 PM
Which device are you using, and is it a Cortex-M0+ or a 'plain' Cortex-M0 ?
I hate breaking bad news to people, but it may at least save you a lot of trouble.Normally, the Cortex-M0 does not allow moving the vector table.The Cortex-M0+ does allow moving the vector table, though; to do this, you'll need to modify the VTOR hardware register.Please let us know the name of the device, which you're trying to move the vector table for.2015-06-19 7:56 PM
Normally, the Cortex-M0 does not allow moving the vector table.
That is exactly why you can change the memory that is shadowed at the zero memory base. A technique that's been in use for at least 3 decades.The issue here is what the content of the table is, whether the NVIC has been setup or if there's any exception vectors (Hard Fault) to catch anything else.2015-06-19 8:30 PM
Sorry for the noise, I completely forgot about remapping; thanks for waking me up! :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.