2024-04-12 2:10 AM
Hi there,
I wrote some data to the Nand Flash which is extended by FMC.
The address of Nand Flash is 0x70000000 in STM32F429BIT6.
I can read the Nand Flash data by HAL_NAND_Read_Page_8b() correctly.
But when I access the data by memory map mode, the data is an error.
I test by this code sniped:
uint8_t rBuf[2048] = {0};
NAND_AddressTypeDef nand_addr = {.Page = 0, .Block = 0, .Plane = 0};
HAL_NAND_Read_Page_8b(&hnand1, &nand_addr, rBuf, 1);
LOG_DBG("read Nand %02x\n", rBuf[5]);
LOG_DBG("read Nand 0x70000005 = %02x\n", *(uint8_t*)0x70000005);the result as below:
read Nand 05
read Nand 0x70000005 = FFI config the FMC to FMC_NAND_BANK2, whose address is 0x70000000.
Why this happened?
Do I need to enable the memory map mode for the Nand Flash?
Thanks for your help!
2024-04-14 6:09 PM
I try this code in my STM32H743II MCU, the result is the same.
Does the Nand Flash NOT support the memory map access mode?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.