2021-11-26 2:46 AM
I have code on L4 series that i want to run on L0 series. what are the changes and where that changes i have to make in order to make code runnable. I think with STM32 back word compatibility is there can any one guide me how to do that.
2021-11-26 2:58 AM
You could check AN4809 Migrating between STM32L0 Series and STM32L4 Series / STM32L4+ Series microcontrollers
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-11-26 3:13 AM
Thanks @Peter BENSCH
i have gone through the document they have give hardware level how can i do l4 series code runnable with L0 where and in which file i have to make changes in the at the software level.
2021-11-26 7:12 AM
C code is generally transferrable. You haven't specified what you program does or what MCU features it uses, so it's anybody's guess as to what you need to change, if anything.
2021-11-26 8:00 AM
Generally, work through the hardware differences, identify piece(s) software which is (are) related to given difference, and modify that piece of software as needed.
JW
2021-11-29 12:18 AM
I have code C:\Users\nikhi\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-BLE1\6.2.2\Projects\Nucleo-L476RG
this project code i want to run on Nucleo-L073RZ how to do that
@TDK @Peter BENSCH @Community member
2021-12-13 7:51 AM
Hi @Nikhil Gayke ,
Hope not too late.. or may be you already found solution since your initial post.
X-CUBE-BLE1 is a SW package compatible with CubeMX. You can easily generate code for your NUCLEO-L073.
Here attached is a GettingStarted document. This doc is of course available directly from CubeMX while using X-CUBE-BLE1 SW pack.
Regards,
Seb.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.