STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have bought a batch of STM32F750N8 MCU's and have found that the following pins do not work. PB14, PB15, and PA12/PA11.

I have tried turning these pins to GPIO's and tried toggling them, however, they seem to just be floating. I can confirm that these pins have been soldered on properly, since I have checked them using an X-RAY inspection system. I can also confirm th...

PMold.1 by Associate III
  • 1675 Views
  • 4 replies
  • 2 kudos

what isITR0, ITR1 how do I set it up

I see that times can be initiated by ITR0, ITR1 in CubeMX etc. I understand that it is internal interrupt. I do not how to set for example another timer to turn another timer on and off.I do not see in CubeMX any option to setup one timer as global i...

MNapi by Senior III
  • 13984 Views
  • 7 replies
  • 15 kudos

Resolved! CAN Bus 2.0 and CAN bus FD

We have developed our control system around CAN bus 2.0, but we are trying to move up to the H7, and it only has CAN FD. The question is, can CAN bus FD be configured for operating like CAN bus 2.0?

IAgui by Associate III
  • 4641 Views
  • 7 replies
  • 0 kudos

We intend to use STWBC2-HP in our PCB. We would like to use circuit "Qi single coil, fixed frequency full-bridge, USB powered". However, we could not identify components used. Do you have any schematic with higher detail level of details?

We intend to use STWBC2-HP in our PCB. We would like to use circuit "Qi single coil, fixed frequency full-bridge, USB powered". However, we could not identify components used. Do you have any schematic with higher detail level of details (such as res...

De init peripherals to jump another app

I am writing a code to jump to another application in the flash. In the last step I am initiating peripherals. My question is related if it is sure to de init peripherals without disable the peripheral first. Example: LL_CRC_DeInit(CRC); LL_AHB1_GRP...

JCuna.1 by Senior
  • 3381 Views
  • 3 replies
  • 2 kudos

GPIO Analog Mode vs Alternate Function ADC

Hello,I am trying to do a voltage measurement, i know i can use ADC to do it. What a gpio is capable of when it is configured as Analog Mode? Can it measure voltages? or Can it trigger an interrupt if a defined threshold exceeds?I need a clarificatio...

How to clear the SPI RX FIFO (register mode)

Hi all, I have an issue. I need to see the Slaves free space, for that, I am reading the slave's Empty space, and based on the results I send the data points which needed. but I am having a big issue. it always has a one execution cycle delay. For ex...

Roshan by Associate III
  • 4150 Views
  • 4 replies
  • 0 kudos

BlueNRG_LP multiple channel ADC

I am working with BlueNRG LP.I am acquiring 3 channels:ADC_VINP0 (PB3)ADC_VINM0 (PB2)BATTERY.I used and modified example of the "BlueNRG-LP Navigator" ADC_DMA.I read ADC_VINP0 and the batteries but ADC_VINM0 not work!! ( I used STEVAL-IDB011V1 and i ...

Hi im working on stm32l072cbt6 micro controller im trying to read the adc value on channel1 in polling method i generated the code using stm32 cube ide,the issue is that always i could not se any variation in the adc raw values and my code is as below,

void MX_ADC_Init(void) {   /* USER CODE BEGIN ADC_Init 0 */   /* USER CODE END ADC_Init 0 */   ADC_ChannelConfTypeDef sConfig = {0};   /* USER CODE BEGIN ADC_Init 1 */   /* USER CODE END ADC_Init 1 */ /** Configure the global features of ...

NJP.1 by Associate III
  • 2491 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.