2015-06-10 2:34 PM
Hi,
We want to add a cell battery to keep time and date. but in the schemaitcs, Pin 1 and Pin 6 in STM32F429iDisco for VBAT alredy connect to +3V.What we can do?Thanks a lot2015-08-20 10:37 AM
I have an STM32F429I-DISCO with an LSE, added as described earlier. The clock starts and runs for me.
Not sure where you're implementation is falling over. If you need consulting work done on this, please contact me off board.2015-08-20 10:54 AM
Attached is a small test app that turns on the LSI and LSE, and benchmarks them against the 8 MHz HSE source.
The software outputs via the SWV (use ST-LINK SWV Viewer) at 180 MHzTest
SYS:180000000 H:180000000, P1:45000000, P2:90000000
PLL Source
PLL using HSE
HSI Running
HSE Running
PLL Running
WARNING: PLL I2S Not Ready
WARNING: LSI Failed to start
LSE Running
SYSTICK:180000
STM32 2048 KB FLASH, 256 KB RAM, 002D001B-3432470C-30333837 UNIQUE
ClockDiagnostic
SYS:180000000 H:180000000, P1:45000000, P2:90000000
LSI:32216, LSE:32764
PLL Source
0 32766
1 32765
2 32765
3 32765
4 32765
5 32765
6 32765
7 32765
8 32765
9 32765
SYS:180000000 H:180000000, P1:45000000, P2:90000000
PLL Source
PLL using HSE
HSI Running
HSE Running
PLL Running
WARNING: PLL I2S Not Ready
LSI Running
LSE Running
SYSTICK:180000
STM32 2048 KB FLASH, 256 KB RAM, 002D001B-3432470C-30333837 UNIQUE
________________
Attachments : SWV-LSI-STM32F429-DISCO.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I10o&d=%2Fa%2F0X0000000bj3%2F3nqyllAKFcR0eRaZujIDIgRdFxyMx_pUoEDe0dNgpO8&asPdf=false
2015-08-21 2:52 AM
Dear clive1,
I try to contact you off board.But I am not able to find your contact info. Do you mind to send me email: linda.li8933@yahoo.caThanks2015-12-31 1:54 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.