2015-06-10 2:34 PM
Hi,
We want to add a cell battery to keep time and date. but in the schemaitcs, Pin 1 and Pin 6 in STM32F429iDisco for VBAT alredy connect to +3V.What we can do?Thanks a lot2015-06-11 7:20 AM
See UM1670, 4.11.2 OSC 32 KHz clock supply, ''Oscillator on board (from X2 Crystal)''
JW2015-06-11 7:37 AM
Yes, PC14/15, needs to be a 6pF crystal, check the BOM
ST commonly uses the EPSON 32.768KHz 6pF part (formerly JFVNY)You should review thoroughly the available documentation, or have your design engineer do so.6.8pF capacitors at C23,C240 Ohm resistors at R53, R54Open SB16,SB172015-06-11 5:57 PM
Dear Sir,
I have soldered those parts on the PCB, but no matter I open or close SB 16 and SB17, the time has not been updated.What is wrong? Do I need to do anything in coding/program? Why I need to open SB16/SB17, after open them, the crystal connects to no where.Thanks2015-06-11 8:13 PM
Doesn't the SB just disconnect the STM32 from the pin header? This is done so the leads to the crystal a very short.
You should enable the LSE, and check that it starts and oscillates correctly.You would need to select it as a source for the RTC.You'd need to place the device in STANDBY, and make sure the code detects a reset out of standby, and not completely reinitialize the RTC. You could set the alarm to periodically exit standby, or use wakeup.2015-06-13 5:10 AM
If I put the device on
standby mode, the LCD is on, it take a lot of battery. how to shut of LCD?
Thanks2015-06-13 9:56 AM
It's not designed to do that, you'd need to gate the primary supply at the regulator, probably.
It sounds like you need to design a custom board with the feature set you require.2015-06-14 6:09 AM
I tried to put the device on STOP mode. But it can not wake up. Here is code I use:
int8_t RTC_Configuration(void){ RTC_Error = 0; EXTI_InitTypeDef EXTI_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* Enable the PWR clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); /* Allow access to RTC */ PWR_BackupAccessCmd(ENABLE);#if defined (RTC_CLOCK_SOURCE_LSI) /* LSI used as RTC source clock*//* The RTC Clock may varies due to LSI frequency dispersion. */ /* Enable the LSI OSC */ RCC_LSICmd(ENABLE); /* Wait till LSI is ready */ while(RCC_GetFlagStatus(RCC_FLAG_LSIRDY) == RESET) { } /* Select the RTC Clock Source */ RCC_RTCCLKConfig(RCC_RTCCLKSource_LSI);#elif defined (RTC_CLOCK_SOURCE_LSE) /* LSE used as RTC source clock */ /* Enable the LSE OSC */ RCC_LSEConfig(RCC_LSE_ON); /* Wait till LSE is ready */ while(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET) { } /* Select the RTC Clock Source */ RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);#else #error Please select the RTC Clock source inside the main.c file#endif /* RTC_CLOCK_SOURCE_LSI */ /* Enable the RTC Clock */ RCC_RTCCLKCmd(ENABLE); /* Wait for RTC APB registers synchronisation */ RTC_WaitForSynchro(); /* RTC Wakeup Interrupt Generation: Clock Source: RTCCLK_Div16, Wakeup Time Base: ~4s Wakeup Time Base = (16 / (LSE or LSI)) * WakeUpCounter */ RTC_WakeUpClockConfig(RTC_WakeUpClock_RTCCLK_Div16); RTC_SetWakeUpCounter(0x1FFF); /* Enable the Wakeup Interrupt */ RTC_ITConfig(RTC_IT_WUT, ENABLE); /* Connect EXTI_Line22 to the RTC Wakeup event */ EXTI_ClearITPendingBit(EXTI_Line22); EXTI_InitStructure.EXTI_Line = EXTI_Line22; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); /* Enable the RTC Wakeup Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = RTC_WKUP_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Calendar Configuration with LSI supposed at 32KHz */ RTC_InitStructure.RTC_AsynchPrediv = 0x7F; RTC_InitStructure.RTC_SynchPrediv = 0xFF; /* (32KHz / 128) - 1 = 0xFF*/ RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_24; RTC_Init(&RTC_InitStructure); /* Get the LSI frequency: TIM5 is used to measure the LSI frequency */ LsiFreq = GetLSIFrequency(); /* Adjust LSI Configuration */ RTC_InitStructure.RTC_AsynchPrediv = 0x7F; RTC_InitStructure.RTC_SynchPrediv = (LsiFreq/128) - 1; RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_24; RTC_Init(&RTC_InitStructure); return RTC_Error;}static void SYSCLKConfig_STOP(void){ /* After wake-up from STOP reconfigure the system clock */ /* Enable HSE */ RCC_HSEConfig(RCC_HSE_ON); /* Wait till HSE is ready */ while (RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET) { } /* Enable PLL */ RCC_PLLCmd(ENABLE); /* Wait till PLL is ready */ while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) { } /* Select PLL as system clock source */ RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); /* Wait till PLL is used as system clock source */ while (RCC_GetSYSCLKSource() != 0x08) { }}main { STM_EVAL_PBInit(BUTTON_USER, BUTTON_MODE_EXTI); while (1) { /* Insert 5 second delay */ GUI_Delay(5000); /* Turn OFF LED4 */ STM_EVAL_LEDOff(LED4); /* Enable Wakeup Counter */ RTC_WakeUpCmd(ENABLE); /* Enter Stop Mode */ PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFI); /* Disable Wakeup Counter */ RTC_WakeUpCmd(DISABLE); /* Configures system clock after wake-up from STOP: enable HSE, PLL and select PLL as system clock source (HSE and PLL are disabled in STOP mode) */ SYSCLKConfig_STOP(); }}2015-06-14 7:00 AM
You might want to work on a more linear initialization sequence.
Measure the frequency after the LSI starts, then init the RTC (once), the init the WakeUp (after).2015-06-14 9:03 AM
Check the LED3 and LED4, it seems wake up. just can not go back where it was.
Then I tried add these code following, then it can not wake up.: JumpAddress = *(__IO uint32_t*) (0x08000000 + 4); Jump_To_Application = (pFunction) JumpAddress; __set_MSP(*(__IO uint32_t*) 0x08000000); Jump_To_Application();It becomce like that, then it can not wake up.static void SYSCLKConfig_STOP(void){ /* After wake-up from STOP reconfigure the system clock */ /* Enable HSE */ RCC_HSEConfig(RCC_HSE_ON); /* Wait till HSE is ready */ while (RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET) { } /* Enable PLL */ RCC_PLLCmd(ENABLE); /* Wait till PLL is ready */ while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) { } /* Select PLL as system clock source */ RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); /* Wait till PLL is used as system clock source */ while (RCC_GetSYSCLKSource() != 0x08) { } JumpAddress = *(__IO uint32_t*) (0x08000000 + 4); Jump_To_Application = (pFunction) JumpAddress; __set_MSP(*(__IO uint32_t*) 0x08000000); Jump_To_Application();};2015-08-20 8:26 AM
Dear Sir,
I still can not make the LSE work, I can not detect any signal from the crystal. static void RTC_Config(void){ EXTI_InitTypeDef EXTI_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* Enable the PWR clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); /* Allow access to RTC */ PWR_BackupAccessCmd(ENABLE);//#if defined (RTC_CLOCK_SOURCE_LSI) /* LSI used as RTC source clock*////* The RTC Clock may varies due to LSI frequency dispersion. */ // /* Enable the LSI OSC */ // RCC_LSICmd(ENABLE); RCC_LSICmd(DISABLE);// /* Wait till LSI is ready */ // while(RCC_GetFlagStatus(RCC_FLAG_LSIRDY) == RESET)// {// }// /* Select the RTC Clock Source */// RCC_RTCCLKConfig(RCC_RTCCLKSource_LSI);// //#elif defined (RTC_CLOCK_SOURCE_LSE) /* LSE used as RTC source clock */ /* Enable the LSE OSC */ RCC_LSEConfig(RCC_LSE_ON); /* Wait till LSE is ready */ while(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET) { } /* Select the RTC Clock Source */ RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);//#else//// #error Please select the RTC Clock source inside the main.c file//#endif /* RTC_CLOCK_SOURCE_LSI */ /* Enable the RTC Clock */ RCC_RTCCLKCmd(ENABLE); /* Wait for RTC APB registers synchronisation */ RTC_WaitForSynchro(); /* RTC Wakeup Interrupt Generation: Clock Source: RTCCLK_Div16, Wakeup Time Base: ~4s Wakeup Time Base = (16 / (LSE or LSI)) * WakeUpCounter */ RTC_WakeUpClockConfig(RTC_WakeUpClock_RTCCLK_Div16); RTC_SetWakeUpCounter(0x1FFF); /* Enable the Wakeup Interrupt */ RTC_ITConfig(RTC_IT_WUT, ENABLE); /* Connect EXTI_Line22 to the RTC Wakeup event */ EXTI_ClearITPendingBit(EXTI_Line22); EXTI_InitStructure.EXTI_Line = EXTI_Line22; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); /* Enable the RTC Wakeup Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = RTC_WKUP_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.