2015-12-31 12:31 PM
Hi guys!
Is it possible to use only assembler startup code without any libraries to create project for STM32F7? When I'm trying to include SystemInit() function in stm32f7xx.c file, I must include core_cm7.h header file. Is it possible to use only .s and .c/.h files to start the project?2014-12-31 7:44 PM
Of course it's possible to do any number of things. One could create a completely functional system from a single .S file, the processor simply starts executing code from the ResetHandler on forward. If you don't want to use other files, you can chose not to do that, and create your own defines or equates.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.