2014-03-14 8:03 AM
If someone could give me an idea, that'd be great. I need it to speed up math operations.
2014-03-14 8:21 AM
Don't some of the template projects do so? Probably buried in a compiler/target option pane some place.
Remember the FPU supports only 32-bit float operations, ie sqrtf(), cosf(), etc The FPU is typically physically enabled in SystemInit() within system_stm32f4xx.c, note the defines the compiler generates when the FPU is enabled, this likely also impacts the libraries pulled in by the linker.void SystemInit(void)
{
/* FPU settings ------------------------------------------------------------*/
#if (__FPU_PRESENT == 1) && (__FPU_USED == 1)
SCB->CPACR |= ((3UL << 10*2)|(3UL << 11*2)); /* set CP10 and CP11 Full Access */
#endif
//..
2014-03-14 8:40 AM
Hi
Right click on the project and select properties. Open the ''C/C++ Build'' on the left hand panel. Select ''Settings'' in the left hand panel. In the main panel - select the ''Tool Setting'' panel (2nd one along) This should list the settings for Assembler, C Compiler, C linker, Other Open the C Compiler list and select ''Target'' In the panel : there should be ''Floating point'' and ''FPU'' drop downs. In the FPU drop down select ''FPV4-SP-D16'' BE WARNED - if you change the processor - it will wipe ALL the other settings! This is a known problem with Atollic/Eclipse2024-05-24 8:00 PM
left click to properties section --> on left side select C/C++ build. look for Tool Settings tab and inside that click on MCU settings. look out for Floating - point unit options and select "None". Below that select Floating-point ABI as "Software Implementation".
I hope that helps :)
2024-05-25 5:31 AM
Only a decade late...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.