2017-06-22 12:07 AM
hello ,
How to configure the DFU ( bootloader USB ) on stm32f7 ?
2017-06-22 1:41 AM
Hi
youssef.elmzaiti
,I recommend you to have alook to :
Please refer to UM0412,
USB device firmware upgrade STMicroelectronics extension for more details on the driver installation and PC host user interface.-Nesrine-
2017-06-22 8:16 AM
Hi Nisrina
we want to migrate from stm32f4xx to stm32f7xx , so this program bootloader DFU on stm32f4xx , it's works , and no on stm32f7xx
void bootloader_DFU_400(void )
{ /* La fonction est compilée uniquement si on est sur un micro STM32F4xx */ typedef void (*pFunction)(void); pFunction Jump_To_Application; vu32 JumpAddress; GPIO_InitTypeDef GPIO_InitStructure; vu8 bouton_DFU;/* Activation Clock GPIO_BP_DFU */
RCC_AHB1PeriphClockCmd( RCC_GPIO_BP_DFU, ENABLE );/* Configuration de PE3 en entrée */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin = PIN_BP_DFU; GPIO_Init( GPIO_BP_DFU, &GPIO_InitStructure );/*
Lecture de l'état du bouton DFU 0 : Bouton DFU appuyé 1 : Bouton DFU relaché */ bouton_DFU = GPIO_ReadInputDataBit( GPIO_BP_DFU, PIN_BP_DFU );/* Si le bouton est appuyé (bouton_DFU = 0) on lance le programme du DFU */
if ( bouton_DFU == 0x00 ) { JumpAddress = *(vu32*) (ADRESSE_FLASH_DFU + 4); Jump_To_Application = (pFunction) JumpAddress;RCC->APB2ENR = 0x00004000; //ChL 15/04/2016 besoin de ces 2 lignes pour les micros serie F42x et supérieurs
SYSCFG->MEMRMP = 0x00000001; //ChL 15/04/2016 besoin de ces 2 lignes pour les micros serie F42x et supérieurs/* Initialize user application's Stack Pointer */
__set_MSP(*(vu32*) ADRESSE_FLASH_DFU); Jump_To_Application(); } else { if (((*(vu32*)ApplicationAddress) & 0x2FFE0000 ) == 0x20000000) { /* Jump to user application */ /* Test if user code is programmed starting from address 0x8004000 */ /* Jump to user application */ JumpAddress = *(vu32*) (ApplicationAddress + 4); Jump_To_Application = (pFunction) JumpAddress; /* Initialize user application's Stack Pointer */ __set_MSP(*(vu32*) ApplicationAddress); Jump_To_Application(); } } }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.