2021-10-26 11:46 PM
Hi, I'm doing motor drive project using F429. I want to achieve ADC triggered by PWM edges and generate interrupt to deal with ADC results, Timer 1 is counting-up mode, so How to configure related registers?
ADC triggered at one (only one at one timer period) of falling edge of T1's CC1 , CC2 and CC3, as a result, CC1 +CC2+CC3 trigger ADC in turns.
Thank you in advance.
2021-10-27 12:35 PM
I don't understand the problem description. Try to draw a timing diagram, indicating the observed behaviour and also the expected one. You may also want to read out and check/post TIM and ADC registers content.
JW
2021-10-27 5:11 PM
Hi, thanks for your kind reply.
the frequency of Timer 1 is 10khz, its CC1+CC2+CC3 comparators output complementary PWMs, CC4 is configured to be some value equal to CC1~CC3, using CC4 falling event to trigger ADC ,then read out ADC registers (or transfer DR register by DMA) and do filtering operation at the end of conversion.
2021-10-27 8:08 PM
*********************************************************
this is ADC interrupt handler:
*********************************************************
this ADC interrupt hits Line 750 three times during one TIMER1 period, however, I just want one hit at LINE 750 after ADC sampling which triggered by T1 CC4 event.
this is part of my init function :
/* ADC2 init function */
void MX_ADC2_Init(void)
{
ADC_ChannelConfTypeDef sConfig = {0};
ADC_InjectionConfTypeDef sConfigInjected = {0};
hadc2.Instance = ADC2;
hadc2.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV6;
hadc2.Init.Resolution = ADC_RESOLUTION_12B;
hadc2.Init.ScanConvMode = DISABLE;
hadc2.Init.ContinuousConvMode = ENABLE;
hadc2.Init.DiscontinuousConvMode = DISABLE;
hadc2.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc2.Init.NbrOfConversion = 1;
hadc2.Init.DMAContinuousRequests = ENABLE;
hadc2.Init.EOCSelection = ADC_EOC_SEQ_CONV;
// hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
// hadc2.Init.ExternalTrigConv = ADC_SOFTWARE_START;
if (HAL_ADC_Init(&hadc2) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_10;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_15CYCLES;
if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
{
Error_Handler();
}
sConfigInjected.InjectedChannel = ADC_CHANNEL_10;
sConfigInjected.InjectedRank = 1;
sConfigInjected.InjectedNbrOfConversion = 1;
sConfigInjected.InjectedSamplingTime = ADC_SAMPLETIME_3CYCLES;
sConfigInjected.AutoInjectedConv = ENABLE;
sConfigInjected.InjectedDiscontinuousConvMode = DISABLE;
sConfigInjected.InjectedOffset = 0;
sConfigInjected.ExternalTrigInjecConvEdge = ADC_EXTERNALTRIGINJECCONVEDGE_FALLING;
sConfigInjected.ExternalTrigInjecConv = ADC_EXTERNALTRIGINJECCONV_T1_CC4;
if (HAL_ADCEx_InjectedConfigChannel(&hadc2, &sConfigInjected) != HAL_OK)
{
Error_Handler();
}
HAL_ADCEx_InjectedStart_IT(&hadc2);
__HAL_ADC_DISABLE_IT(&hadc2, ADC_IT_JEOC);
HAL_ADC_Start_DMA(&hadc2,(uint32_t *)u16ADC2_Buf,ADC2_NUM_MAX);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.