STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About Viewing source code of libraries used

I am using STM32L4 series microcontroller. I am debugging some code which uses standard C lib function fopen() and fread(). The code can be compiled and has no errors. For some reason fopen() function is returning NULL pointer when used. I wanted to ...

SSrid.1 by Associate
  • 2121 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F103 RTC calibration issue

Hi,I'm trying to calibrate my RTC by writing on the RTCCR register on an STM32F103 MCU. However, it seems like this is not taken into account as the 512Hz signal is still slightly out.I'm using the following code:PWR-> CR |= PWR_CR_DBP; // Allow acce...

LRegn.11 by Associate II
  • 2024 Views
  • 2 replies
  • 0 kudos

STM32F417 CAN Filtering

Heei,See figure 342 on page 1088 on reference manual RM0090 Rev 19. It denotes the 32-bit CAN filter register layout. I have the registers configured as described below:F1 register is 0x200000 (bit 21 set). e.g. stdid[0]F2 register is 0x1fe00000 (bit...

Jenny by Associate II
  • 1649 Views
  • 2 replies
  • 0 kudos

What FMAC can do?

I want to do averaging, and finding peak value of about 1k ADC readings. I wonder if I can use FMAC to do it to offload MCU .

HDaji.1 by Senior
  • 1699 Views
  • 2 replies
  • 0 kudos

Resolved! Timer slave trigger polarity for input capture

I want to use TIM1_CH1 to measure pulse width. TIM1 works under slave reset mode. The input trigger is TI1FP1. Ideally, TIM1 resets upon rising input, then TIM1_CH1 captures the falling edge. The CCR1 value would be the pulse width. The problem is th...

Yuan1 by Associate II
  • 5546 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.