2015-05-06 4:03 AM
I want to have a sample of system clock at MCO pin of STM32F107RC micro controller.
I use dspin firmware library for driving stepper motor. The on board crystal is 8MHz and system clock set to be 72MHz. I add this code to ''dspin.c'': GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); and I add the below line code in ''SetSysClockTo72()'' function at ''system_stm32f10x.c'' file. RCC->CFGR &= (uint32_t)0xF6FFFFFF; //HSE clock selected as MCO source But I don't have no clock output on this pin. please guide me thanks yasamin2015-05-15 3:20 AM
Hi Clive,
Thanks for your explanation.Yes it is possible to remove post.But as a general rule that we may apply here: keep only one topic on once discussion.This way, it will be easier for other users to find a help and then for contributors to follow the discussion.Don't you agree?-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.