STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L051K8 Standard Peripheral Library

Posted on May 15, 2015 at 16:52Hi all,Throughout my time programming STM32 microcontrollers, I've used the standard peripheral libraries. Having recently designed my latest product around the STM32L051K8, I thought there would be a standard peripher...

harris by Associate II
  • 1526 Views
  • 2 replies
  • 0 kudos

STM32F4 waking up from STANDBY by RTC alarm

Posted on May 11, 2015 at 15:27Hi,I have a big problem with waking up the STM32F4 MCU from STANDBY mode by RTC alarm and I dont see any solutions...The problem is that the MCU wakes up only sometimes from the RTC Alarm. Usually like 3 times in a row...

32F429IDISCOVERY Waking up from STANDBY by RTC alarm issue

Posted on May 07, 2015 at 21:38Hi,I have a big problem with waking up the 32F429IDISCOVERY board from STANDBY mode by RTC alarm and I dont see any solutions...The problem is that the board wakes up only sometimes from the RTC Alarm. Usually like 3 t...

STM32F4 I2C send NACK if received byte == 0

Posted on May 13, 2015 at 13:26Hi everyone, I want to interface an STM32F429IIT to a SI4735 radio chip using the I2C interface. The SI4735 programming manual says, the status bytes should be read after sending a command. My problem is, that the firs...

stm32f401 USB schematic

Posted on May 14, 2015 at 16:09Good day,I want to make stm32f401 act like slave for my project.Can you tell if this schematic will work?

0690X000006031kQAA.jpg
hitsumen by Associate II
  • 928 Views
  • 1 replies
  • 0 kudos

STM32 and Audio for SIM900

Posted on May 15, 2015 at 14:04I need my device to call a number using the SIM900 GSM chip and play a *.wav file from the flash to the SIM900's microphone. I have no experience with audio and I have 2 questions: 1. Is it possible to use microcontrol...

Blinking LED

Posted on May 15, 2015 at 08:02Hello everyone,    i would like to ask for your knowledge. I am new in Cortex programming (my only experience is on Adruino platform) and i have managed to blink the LEDs on my Cortex device (it's an STM32 conStick fro...

pmamatsis by Associate II
  • 1574 Views
  • 2 replies
  • 0 kudos

32F429IDISCOVERY SDRAM(FMC) and PG2 pin problem

Posted on May 14, 2015 at 18:09Hi,I have a very strange problem with the SDRAM controlling and PG2 pin use. I use SDRAM as an additive memory space so it is vital for my program because I do calculations that need a lot of space. This works very wel...

how to allow the clock to be output onto the external MCO pin

Posted on May 06, 2015 at 13:03I want to have a sample of system clock at MCO pin of STM32F107RC micro controller. I use dspin firmware library for driving stepper motor. The on board crystal is 8MHz and system clock set to be 72MHz. I add this code...

yasamin by Associate II
  • 4304 Views
  • 10 replies
  • 0 kudos

STM32F407: Can I turn off LD1 COM and LD2 PWR LEDs?

Posted on May 15, 2015 at 07:22Hi,I am trying to do a project for school, where I am just trying to measure the power consumption of the board running my algorithm, but I would like to measure the board with ALL LEDs off. I was wondering if it's pos...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.