2020-05-08 4:34 AM
Board : STM32F767 Nucleo-144
Environment : Raspberry PI model B-V1.2
OS : Raspbian
Issue : How I can access STM32 SD card from Raspberry PI model B-V1.2 ?
I try to access SD card as share drive from My rasbery pi and I have followed below steps on Raspbian OS:
In order to install the ST-Link utilities on Rasbery Pi, we have to make sure to have the libusb-dev library installed.
1. $ sudo apt-get install libusb-1.0-0-dev
We will now download, build and install the latest ST-Link utilities from scratch
2. $ git clone https://github.com/texane/stlink stlink.git
3. $ cd stlink
4. $ make
5. #install binaries:
6. $ sudo cp build/Debug/st-* /usr/local/bin
7. #install udev rules
8. $ sudo cp etc/udev/rules.d/49-stlinkv* /etc/udev/rules.d/
9. #and restart udev
List all visible drives on the system:
10. $ sudo fdisk -l
And it should be one of /dev/sdb1 or /dev/sdb2.
Make a directory into which you'll mount the USB drive:
11. $ mkdir /media/usb
Mount the USB drive:
12. $ sudo mount /dev/sdb2 /media/usb
13. $ cd /media/usb
But I cannot access images stored in USB, Why ?
Am I missing any critical steps ?
2020-05-08 4:41 AM
What's the ST-LINK got to do with accessing an SD card on an STM32 board?
You'd need an SD card attached, and build a USB MSC device to provide access.
The faux mass-storage on the mBed platform allows you to drop a binary file as a means of burning firmware to the STM32, not create directories and add random content.
2020-05-08 10:19 PM
Thanks for your inputs.
I am newbie on ST board.
so kindly provide more inputs on how to build a USB MSC device ?
2020-05-11 12:42 AM
You find some files in the ST code of the Cube Firmware
i.g: C:\ST\STM32Cube_FW_H7_V1.6.0\Middlewares\ST\STM32_USB_Device_Library\Class\MSC
Kind regards
Daniel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.