2026-03-31 3:55 AM - last edited on 2026-03-31 6:48 AM by mƎALLEm
I am using an STM32 Nucleo-F767ZI with RMII Ethernet + LAN8742A PHY and an example project based on lwIP/TCP-IP.
I noticed a strange behavior: if I comment out MX_USB_OTG_FS_PCD_Init(), Ethernet communication stops working. If I keep it enabled, Ethernet works correctly.
The peripheral initialization order is:
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_LWIP_Init();
MX_TIM3_Init();
MX_SPI4_Init();
MX_CAN1_Init();
MX_UART5_Init();
MX_USB_OTG_FS_PCD_Init();
Additional observations:
SystemClock_Config() does not change
Replacing MX_USB_OTG_FS_PCD_Init() with HAL_Delay() does not fix it
So it does not look like a timing issue
It seems that HAL_PCD_Init() / HAL_PCD_MspInit() for USB is enabling or configuring something indirectly that Ethernet depends on
My question is:
What could USB FS initialization be configuring that would make Ethernet work, even though they should be unrelated?
I am thinking about possibilities such as:
GPIO clocks being enabled indirectly
MSP/NVIC configuration side effects
Some indirect dependency affecting HAL_ETH_MspInit() or lwIP
Has anyone seen something similar with STM32F767 + LAN8742A + lwIP?
Solved! Go to Solution.
2026-04-01 8:51 AM
Hello @BTurc.2,
After analysis, it appears the issue is related to LwIP misconfiguration, particularly the LwIP RAM heap pointer address. I made several adjustments:
#define MEM_SIZE 16*1024
Regarding the function being commented out or uncommented, the issue might be related to memory alignment or a similar cause. I have been pinging the app nonstop, and everything seems to work well.
Additionally, please refer to this article for further details and as a reference for future work:
Best regards,
2026-03-31 4:01 AM
Hello @BTurc.2,
This is unusual. I cannot say for sure without analyzing the application in depth. Could you please attach your project so I can review it? If the project is private, feel free to send me a private message, and I can provide a secure line for you to upload the project.
Best regards,
2026-03-31 5:07 AM - last edited on 2026-03-31 7:01 AM by STackPointer64
Hello @STackPointer64,
My project is derived from the following repository:
https://github.com/ahmetkcavusoglu/nucleo-f767zi_lwip
With the original repository, TCP/IP communication with the Nucleo works correctly even when MX_USB_OTG_FS_PCD_Init(); is fully commented out.
Since my project is private, I will send it to you by private message.
In my project, I observed the following behavior inside MX_USB_OTG_FS_PCD_Init():
I can comment out all the initialization code and TCP/IP communication still works, as long as this line remains present:
hpcd_USB_OTG_FS.Instance = USB_OTG_FS;
If that line is also removed, the board is no longer reachable over TCP/IP.
So at the moment it seems that the issue is not related to full USB OTG FS initialization itself, but rather to some side effect associated with assigning the USB instance to the PCD_HandleTypeDef.
2026-04-01 8:51 AM
Hello @BTurc.2,
After analysis, it appears the issue is related to LwIP misconfiguration, particularly the LwIP RAM heap pointer address. I made several adjustments:
#define MEM_SIZE 16*1024
Regarding the function being commented out or uncommented, the issue might be related to memory alignment or a similar cause. I have been pinging the app nonstop, and everything seems to work well.
Additionally, please refer to this article for further details and as a reference for future work:
Best regards,
2026-04-02 12:56 AM
Hello @STackPointer64 ,
I changed LWIP_RAM_HEAP_POINTER to 0x20074000 and increased MEM_SIZE to 16*1024. It is now working correctly.
Thank you very much for your help! Best regards!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.