2010-03-23 6:32 AM
How many Encoders can be read at same time
2011-05-17 4:44 AM
Depends on frequency of signals.
If they are very fast (100kHz -> 10 MHz), you have to use timers in encoder mode. In such case each timer can handle one encoder and each such timer needs CC1 & CC2 or CC3 & CC4. So you have to check the datasheet and search, which timers have either of these CC pairs available. For lower frequencies, you may use a combination of above method and some external interrupt sampling (with lower resolution, probably) with a SW counting pulses in interrupts.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.