2010-03-23 4:03 AM
Sources of internal bootloader on STM32F10x
2011-05-17 4:44 AM
The source code for internal bootloader is not public.
The full source code for DFU bootloader (separately available) is in USB developer kit on st.com/mcu as one of the USB examples.2011-05-17 4:44 AM
AN3154, AN3155 and AN3156 are NOT talking about the internal bootloader. The internal bootloader is described in AN2606.
I have only the reengineered version of the internal bootloader. But this code won't help for a bootloader in C/C++, because it is written to fit into 2k bytes of internal flash and only supports UART1. I don't know, if the source code of the DFU-firmware is available. I think, you want this firmware code and not the internal firmware code.2011-05-17 4:44 AM
Thinks for your answer
But I need sources for USB HOST whereas all sources of application notes on ST website are for USB Device. Do you know where I can find these sources ?2011-05-17 4:44 AM
Basic drivers on register level are in newest USB library, but USB host functionality is not there yet. STOne-32 has pointed out in former article the list of partners, that offer USB host solutions.
Nothing really free from ST does exist yet, except some preliminary code capable of reading the descriptors (a Linux usb driver porting), look more in STM32 forums for it.2011-05-17 4:44 AM
So it's not a good news for us...
But canwe imagine ask to STOne32 the sources of demonstrations like UM0721 or UM0412 ? Or can we imagine to pay for these sources ? We needabsolutely an
exemple of code to develop our application. We have no idea how to read files on Mass storage... Do you know who we could ask for this and price ? Thanks a lotWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.