2018-07-30 5:59 AM
I made an integer Square root function:
int integerSQRT, result,result2;
for (integerSQRT = 0; integerSQRT < 100; integerSQRT++)
if (integerSQRT*integerSQRT >= squaredResult) {
result = integerSQRT - 1; // just larger than the sqroot -1 is just less than
integerSQRT = 100;
}
// easily adapted to cube root, quad root etc...
Solved! Go to Solution.
2018-07-31 4:47 PM
by halving the initial guess (similar to the cordic approach), I got about 230 ticks (-O1 optimized) to 290 ticks (no optimization) to calculate the integer sqrt of 65535, on a CM0.
running at 48Mhz, that means 5 - 6us per calculation, inclusive of overhead.
see if your code can beat that.
2018-07-30 6:11 AM
Jack Ganssle has published routines in several places over the years.
http://www.ganssle.com/approx-2.htm
The Cortex-M0 is going to do everything relatively slowly. You'd likely want to use the TIM or GPIO methods for benchmarking code execution speeds.
Worth noting however that a 48 MHz STM CM0 will not run twice as fast as a 24 MHz one. The flash wait state becomes pretty dominant.
2018-07-30 7:00 AM
just mapping the touch sensors,
to adjust for heavy Vs light touch readings, I needed to use Sqrt(); quickly..
2018-07-30 9:42 AM
the standard math lib is pretty slow. try this:
2018-07-30 12:36 PM
I think you have to show first that your approach works.
Then you have to make a fair comparison: integer to interger math.
From a distance, decrementing the result will be slow. I would halve it, or use a slope based approximation.
Benchmarking it is a piece of cake.
2018-07-30 4:48 PM
just a novel approach, 1000x faster than software Floating Point. as a guess.
2018-07-30 5:39 PM
" as a guess."
yeah. that's the right approach for sure.
2018-07-30 5:54 PM
This integer SQRT works well enough for this problem.
I have 48 channels to transmit every mS or less.
it is only a F0 processor, so I didn't bother to try the double SQRT Math function..
my guess is that it would take at least 1mS in software floating point, that's 1 channel and I have 48 and no time to wait.
I don't need to test it, so I guess...
2018-07-31 3:06 AM
"so I didn't bother to try the double SQRT Math function.."
yet you still claim your algorithm is faster than it. plus, you are compariong integer math vs. double float math: anyone can write the most inefficient integer routines that can beat equivalent 1024-bit most efficient floating math routines.
that's rigorous.
quoting execution time without quoting how fast you run the mcu makes zero sense for an apple to apple comparison.
2018-07-31 4:47 PM
by halving the initial guess (similar to the cordic approach), I got about 230 ticks (-O1 optimized) to 290 ticks (no optimization) to calculate the integer sqrt of 65535, on a CM0.
running at 48Mhz, that means 5 - 6us per calculation, inclusive of overhead.
see if your code can beat that.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.