STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Execution of code in SRAM of STM32F405

Hi, I am using STM32F405.I use the Flash Sector as follows. - Sector 0: IAP - Secotr 2: Data Save - Sector 5: Main ApplicationMain Save the data in APP. And Main_APP erases Sector2 before writing the data.While erasing Sector2 from Main_APP, I notice...

JPark.18 by Associate
  • 1102 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F030RC programming flash problem

HiI have used STM32F030RC.I program the flash memory, using bootloader from PA9 and PA10.I have programmed the microcontrollers first time successfully. But after some program times, I can not program them. I traced the problem. The micro goes to b...

C++ IDE?

Posted on April 10, 2018 at 06:06Anyone has ever tried to install and play with an C++ arduino oriented  IDE that uses arduino libraries but implemented for STM32 micros?Have you ever heard of Sloeber?http://eclipse.baeyens.it/ Seems interesting!

g. lewis by Associate II
  • 9143 Views
  • 22 replies
  • 0 kudos

Nucleo F767ZI - system freeze upon UART ORE interrupt

Hi,My system (MCU) gets into a state where I can't debug it when i get a UART interrupt due to ORE.I even tried placing breakpoints at the places where ORE is captured in the IRQ handler - but the debugger didnt stop and I lost the connection to the ...

I am working with an STM32F405. Planning to use Segger J-link probe and J-scope combination to visualize RAM variables over the JTAG/SWD/SWO interface. does anyone know what is the maximum sampling frequency I can achieve with the STM32F405?

Segger quotes the J-link Ultra+'s target interface speed at 50MHz and an "unlimited sampling bandwidth, limited by the bandwidth of the debug interface"... Ideally I would like to plot 4 floats at atleast 10kHz sampling rate.

sb by Associate
  • 1163 Views
  • 1 replies
  • 0 kudos

Resolved! How fast is a double floating point Square root function on a 48MHz Cortex M0 ?

I made an integer Square root function:    int integerSQRT, result,result2;   for (integerSQRT = 0; integerSQRT < 100; integerSQRT++)        if (integerSQRT*integerSQRT >= squaredResult) {                      result = integerSQRT - 1;      // just l...

T J by Lead
  • 5406 Views
  • 12 replies
  • 0 kudos

How to config SYS_WKUP3 for STM32L4 MCU Standby mode?

Hi,I am setting up STM32L4 for standby mode. From Cube and NUCLEO-L496ZG\Examples\PWR\PWR_SLEEP\Src the GPIO pin is PE6.However I don't see any Cube generated code to init this pin. Neither in example code.Should I init the PE6 as GPIO input pin?Thx ...

Encoder mode and rotary encoder

Posted on April 03, 2018 at 11:10 Hi, I'm using STM32F072RB and a rotary encoder (with 30 dentet) connected to TIM2 in 'encoder mode' and I can see in TIM2->CNT that it is actually counting correctly. I trying to get an interrupt on each detent...

Ariel G by Associate II
  • 11411 Views
  • 24 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.