2022-09-21 4:23 AM
2022-09-21 4:51 AM
Not clear what you're asking.
Initially? Via some user interface, modem or data connection.
To maintain? A battery and an LSE clock crystal.
2022-09-21 5:35 AM
Don't use Cube/HAL (nor SPL).
Simply use the 32-bit RTC counter as a UNIX (or any other) epoch counter, and use the standard C library facilities from <time.h> to convert it to date and time.
JW
2022-09-21 6:00 AM
Hello there
I can save RTC date, but this date is not updated the next day with battery connected
Clock is ok.
2022-09-21 6:09 AM
Not sure I recall all requirements but should be examples in SPL of putting F1 in STANDBY.
Abruptly removing primary power, not so sure.
Need to make sure not to reset/clear RTC at next start.
2022-09-21 6:15 AM
Clive,
the SPL and Cube/HAL implementation of 'F1xx RTC handling is dumb - they limit the RTC to within one day's worth of seconds, and handle date manually, while storing it in one of the backup registers. This of course won't work across midnights with VDD off.
JW
2022-09-21 10:45 PM
Are there any examples of this? Where can I find it , Thanks
2022-09-22 3:08 AM
> Are there any examples of this?
I don't know any.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.