STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F405 bxCAN form errors

I've got a weird situation.We've got a CAN bus going between our controller and a CAT ECU with a couple of PCs watching the conversation going by at about 80 messages per second and we can get a couple of million packets with zero errors. (That's not...

Resolved! Receive parallel data in Nucleo_H743ZI2

HiI am following the AN4666 document to receive parallel gpio data, with on clock input.this is the code I wrote : I was expecting to receive gpio data and save to memory by triggering the DMA at every rising edge my issue is that the timer (input ca...

AElta.1 by Associate II
  • 1415 Views
  • 1 replies
  • 0 kudos

STM32 UART Rx with unknown length

hi i have a problem with my uart program the thing is i have to determine the buffer size of the rx i'll call it rx_buff now i have multiple reception well different messages sizes some times 50bytes some times 2bytes but the problem is that when sen...

bakhti by Associate II
  • 1712 Views
  • 2 replies
  • 0 kudos

STM32H743 – DAC with DMA not working ?

Dear Reader,In this project we’re required to output a DAC signal (to begin with a sine-wave would suffice in terms of proving the code) on PA4 of our STM32H743 micro using DMA.I’ve done some evaluation and testing based on STM’s sample project NUCLE...

TMA1of3 by Associate III
  • 1404 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.