2020-02-21 7:33 AM
it is a processor that is located on a blue & me control unit from fiat
2020-02-21 8:23 AM
Not an STM32
If JTAG is open and unprotected you could likely use a U-LINK or J-LINK.
If it is protected then you'll need to engage people who can recover devices.
Don't expect ST to help you chipping the devices.
2022-05-07 12:34 AM
Hello everyone
I need the bsdl file for this STA2062A device.
I have to develop the jtag test to load the nand Flash on the blue & me fiat control unit
Thanx in advance for the support
Raffaele Coviello
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.