STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to increase GPIO on any STM32 MCU?

I want to design PLC using STM32 MCU so for that I need to extend its GPIO pins how can i do this?Adding another MCU or shift registers any other ideas?Main cpu having MCU and another io modules added is communicate with ​main cpu using protocol like...

Resolved! STM32L0 multi-channel ADC reading has DMA problem

I am trying to read 2 channel ADC with STM32L011F4.My ADC and DMA settings in cubemx are as follows my problem is that the DMA only returns the low 8 bit of the last channel.uint16_t ADC_Reads[2] = {0};   while (1) { HAL_ADC_Start_DMA(&hadc,(uint...

0693W00000NpJS3QAN.png 0693W00000NpJSIQA3.png 0693W00000NpJW0QAN.png

stm32f103c8t6 short cuts after programming!

Hi, I am trying to make a circuit with stm32f103c8t6 and a nrf24l0+. I attach my schematic if pcb layout needed tell me to upload that. One of the circuit work good ( the send one) the other one which is identical does not.after soldering I did check...

0693W000001rxWVQAY.jpg
HSaee.1 by Associate II
  • 9267 Views
  • 19 replies
  • 0 kudos

Resolved! Switching time for mux on Opamp

Various STM32 products have opamps that have a mux in front of it.Ex: STM32G4, STM32F3, STM32H7 series, etc.If I change the mux input setting using the control status register (OPAMPx_CSR::VP_SEL or VN_SEL), how long does it take for the mux to switc...

FMC peripheral memory

How far from FMC shall we place memory device. I have stack-up design(3 boards) in which MCU is on top board and FPGA is on bottom board. I need to map FPGA to FMC. Are there design consideration for routing FMC signals for such board to board commun...

KGane.1 by Associate III
  • 1115 Views
  • 1 replies
  • 0 kudos

FDCAN RX interrupt not firing

Hello, I'm trying to set up an interrupt when my FDCAN controller received a CAN message. MCU is an STM32G01BI went into STCubeMX and I enabled these interrupts:This generated some new functions instm32g0xx_it.c:void TIM16_FDCAN_IT0_IRQHandler(void) ...

0693W00000NpVcLQAV.png

I cannot understand this function "Cunstom_STM_Update_Char" regarding aci_gatt_update_char_value in BLE P2P template example.

I'm following the P2P template example and I found that to send data using BLE, the example uses the Custom_STM_App_Update_Char function. However, as I know the update API is aci_gatt_update_char_value. So, I'm confused because the Custom_STM_App_Upd...

0693W00000NpVbgQAF.png
KKIM.6 by Senior II
  • 973 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.