2019-04-01 1:56 AM
Vref is giving - 5200- 5700 mv but my source is (3300) max
VBAT - 3600 mv
Temp- 170 degrees
not able to get why it giving that difference and my configurations are as per the example cube library
Note: my Vref value is using as VREFANALOG_VOLTAGE for VBAT and Temperature
Thanks in Advance
2019-04-01 8:04 AM
Have you performed the ADC calibration step before running measurements?
2019-04-01 8:47 PM
Yes i performed.
HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.