2025-11-03 5:00 AM - last edited on 2025-11-03 6:37 AM by mƎALLEm
I am currently working on a project that uses the STM32U575CGU3 microcontroller. The goal of the project is to display pressure and temperature values over CAN J1939 and CANopen communication protocols in a digital output format.
For sensor data acquisition, I am using an external two-channel ADC to measure pressure and temperature values.
Regarding the system clock, I have tested the application using both the internal clock source and an external crystal oscillator. The system performs well in both configurations.
However, I would like to request your expert guidance on the recommended clock source for this application. Specifically:
Solved! Go to Solution.
2025-11-03 6:35 AM - edited 2025-11-03 6:45 AM
Hello @sasmitjoshi5 and welcome to the ST community.
No matter CANOpen is used or not. It's recommended to use a Crystal with CAN/FDCAN especially for industrial environment otherwise you will face some communication issues.
See also: Do I need an external crystal for RS485 or CAN on STM32H533RET6?
Hope I've answerd your question.
2025-11-03 6:35 AM - edited 2025-11-03 6:45 AM
Hello @sasmitjoshi5 and welcome to the ST community.
No matter CANOpen is used or not. It's recommended to use a Crystal with CAN/FDCAN especially for industrial environment otherwise you will face some communication issues.
See also: Do I need an external crystal for RS485 or CAN on STM32H533RET6?
Hope I've answerd your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.